Register an Asset Framework (PI-AF) Connector
This topic describes the steps to register an Asset Framework (PI-AF) connector.
NOTE:
In the 1.6.0 release, the Asset Framework (PI-AF) connector is available as a beta version.
Provide Feedback