Delete Role

Perform the following steps to delete a role:
  1. Navigate to the
    Roles Listing
    page and click the role you want to delete.
    The
    Role Detail
    page of the selected role is displayed.
  2. Click
    Delete Role
    .
    The
    Confirm Role Deletion?
    dialog box is displayed. If there are any associated apps or users with the selected role for deletion, you will see a checkbox to acknowledge the removal impact.
  3. Select the
    I acknowledge deletion impact
    checkbox.
    NOTE:
    When you delete a role, it will be removed from the associated apps and users. Before deleting a role, verify the details so that you delete the correct role.
  4. To verify the role deletion, provide the role name in the
    Role Name
    field.
  5. Click
    Delete Role
    .
    To make sure your changes to Roles take effect immediately, log out and log back in.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal