Remove Role

If you are a project administrator, you can remove any assigned roles or all of them.
Perform the following steps to remove the roles:
  1. On the Management Console, select the
    Manage Access
    tab.
  2. In the
    Actions
    column, click the [] icon of the desired users.
    Member Listing
    NOTE:
    If any or all roles are assigned to the member, the [] icon is enabled. If no roles are assigned to the member, the [] icon is disabled.
    The
    Remove Roles
    page displays the assigned roles.
    NOTE:
    Click the [] icon to expand the role and view its capabilities. Click the icon again to collapse it.
    Role Capabilities
  3. Select the checkbox adjacent to a role.
    NOTE: The user can use the search bar to find a specific role.
    You can select multiple roles by selecting the required checkboxes. To remove all the assigned roles, select the
    Roles
    header checkbox.
  4. Click
    Remove
    .
    The "
    Roles updated
    " message is displayed.
    Remove Roles
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal