Navigation

The home page of FactoryTalk DataMosaix features a left navigation menu with the following tabs:
  • Manage Access
  • Extractor Info
  • Applications
  • Modeling
On the left navigation menu, you can also find direct links to Main DataMosaix (Cognite Data Fusion) and FactoryTalk Hub.
Left Navigation Menu
FactoryTalk DataMosaix Tabs
Manage Access
Allows you to modify users' roles using the
Members
sub-tab. You can view, edit, and modify the default and custom
Capability Groups
and
Roles
associated with the organization. Also, you can activate or deactivate a specific functionality in DataMosaix using the
Features
sub-tab.
Extractor Info
Allows you to register extractors that helps to push data to FactoryTalk DataMosaix.
Applications
Allows you to register applications that helps to view data.
Modeling
Allows you to create assets and helps organize assets and their properties in a hierarchical structure.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal