DataMosaix Home Page Header
The home page header has the following options:
- Management Console
- Select Project
- Notifications
- Help and Support
- Profile Settings
DataMosaix Home Page Header

Menu | Description |
---|---|
![]() | Click the FactoryTalk DataMosaix logo to navigate to the Home Page. Clicking the logo displays the Manage Member Access page. |
![]() | You can select a project from the project drop-down list to perform the required operations as per your role. |
![]() | You can view the notifications you receive in FactoryTalk DataMosaix. |
![]() | Click the Help and Support icon to view the following information:
|
![]() | Click the Profile settings icon to view the user name, email address, and the Sign Out option. |
Provide Feedback