Features

This topic describes activating or deactivating a feature in FactoryTalk DataMosaix using the Features tab. Before you activate or deactivate a feature, consider the following:
IMPORTANT:
Only the Project Admins can activate and deactivate the features in a project.
  • By default, the features manageable option on the Features page is inactive. You need to activate them to enable them to be used in DataMosaix.
  • When a feature is deactivated, it becomes unavailable to all users of the selected project.
To view the Features page, on the Management Console, navigate to the
Manage Access
tab and click the
Features
subtab.
Features
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal