Remove Capability

In this section, you will find how to remove a capability associated with a capability group. Only Project Admin users can perform the Remove Capability action and it is only available for custom groups.
The Capability Group Detail page displays the capabilities associated with the selected group as a tile. From the
Capability Group Details
page:
  1. Click
    Remove
    from the capability tile that you want to remove.
    The
    Confirm Capability Removal
    dialog box is displayed and it displays that the selected capability will be queued for removal from the associated roles and users.
  2. To proceed with removing the capability, select the
    I acknowledge removal impact
    checkbox.
  3. Click
    Queue for Removal
    .
    If you do not want to remove the capability, click
    Undo Removal
    . This option will not be available once you save the changes.
    The capabilities queued for removal will be erased from the selected capability group after saving the changes.
  4. Click
    Save
    .
    For the changes to take effect, it is recommended to log out and log back in.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal