Default Capability Groups

The following table displays the list of default capability groups and the associated capabilities with applied actions. When you create a new project in DataMosaix, these capability groups are generated by default. There are 20 default capability groups. You can choose the required capability group from the list based on your requirements and the capabilities and actions applied to it.
The UPDATE capability is not available for FTDM-Grp-Project in order to prevent modifying or removing any OpenID connect-related configuration.
If the default capability group does not fulfill your requirements, you can create a custom capability group to suit your needs. To create a custom capability group, refer to Create a new Capability Group.
NOTE:
Default groups have pre-defined capabilities and these capabilities are not modifiable.
Default Capability Groups
No
.
Default Capability Group Name
Capabilities with applied actions
1
FTDM-Grp-3D
threedAcl: read | create | update | delete
2
FTDM-Grp-AccessManagement
groupsAcI: read | list, extractionPipelinesAcI: read | write
3
FTDM-Grp-Applications
datasetsAcI: read | write, filesAcI: read | write. dataModelsAcI: read, dataModellnstancesAcI: read
4
FTDM-Grp-Chart
assetsAcI: read, timeSeriesAcI: read, filesAcI: read, groupsAcI: list, projectsAcI: list, dataModelsAcI: read, dataModellnstancesAcI: read
5
FTDM-Grp-CogniteApilnputValidations
datasetsAcI: read
6
FTDM-Grp-ContextDiag
filesAcI: read | write, assetsAcI: read | write, eventsAcI: read | write, labelsAcI: read | write
7
FTDM-Grp-ContextEntity
entitymatchingAcI: read | write, assetsAcI: read, timeSeriesAcI: read | write
8
FTDM-Grp-Data
timeSeriesAcl: read, rawAd: read | write, eventsAcI: read | write, assetsAcI: read | write, relationshipsAcI: read | write, filesAcI: read write, sequencesAcI: read | write, transformationsAcI: read | write, sessionsAci: create, projectsAci: list, groupsAci: list, datasetsAci: read | write
9
FTDM-Grp-DataModel
dataModelsAcl: read | write, dataModellnstancesAcI: read | write
10
FTDM-Grp-DataSetsManagement
rawAcI: read | write | list, datasetsAcI: read | write
11
FTDM-Grp-Experimental-Human
scheduledCalculatlonsAd: read | write, monitoringTasksAd: read | write, timeSeriesSubscriptionsAcI: read | write, hostedExtractorsAd: read | write, workflowOrchestrationAcI: read | write
12
FTDM-Grp-Experimental-Machine
scheduledCalculationsAd: read | write, monltoringTasksAcI: read | write, timeSerlesSubscrlptlonsAcI: read | write, hosted ExtractorsAcI: read | write, workflowOrchestrationAcI: read | write
13
FTDM-Grp-Extractor
timeSeriesAcl: read | write, rawAcI: read | write | list, eventsAcI: read | write, extractionRunsAcI: read | write, extractionConfigsAcI: read | write, assets Acl: read | write, relationshipsAci: read | write, datasetsAci: read, filesAci: read | write, sequencesAcI: read | write extractionPipelinesAcI: read | write, transformationsAcI: read | write, groupsAcI: list, projectsAcI: list, sessionsAcI: create, dataModelsAcI: read | write, dataModellnstancesAcI: read | write
14
FTDM-Grp-Function
functionsAcl: read | write, filesAcI: read | write, sessionsAcI: create
15
FTDM-Grp-GenApplications
dataModelsAcl: read | write, dataModellnstancesAci: read | write, assetsAcI: read | write, timeSerlesAcI: read | write, filesAcI: read | write, eventsAci: read | write, sequencesAcI: read | write, labeisAci: read | write, transformationsAcI: read | write, functionsAcI: read | write, projectsAcI: read | list, rawAci: read | list | write, extractionPipelinesAcI: read | write, extractionRunsAci: read | write, extractionConfigsAci: read | write, datasetsAci: read, relationshipsAcI: read | write, sessionsAci: create
16
FTDM-Grp-Media
filesAcl: read, annotationsAcl: write
17
FTDM-Grp-Pipeline
extractionPipelinesAcI: read | write, extractionConfigsAcI: read | write, extractionRunsAcI: read
18
FTDM-Grp-Project *
projectsAcI: read | list
19
FTDM-Grp-Raw
rawAcI: read | write | list
20
FTDM-Grp-ViewApp
projectsAcI: list, dataModelsAcI: read, dataModellnstancesAcI: read, extractionPipelinesAcI: read, extractionConfigsAcI: read
*It is not recommended to update or delete any OpenID connect-related configuration after the project has been created. Because of this, the UPDATE capability of the FTDM-Grp-Project is removed in order to limit access to OpenID connect.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal