Delete Asset

This topic provided information about how you can delete an asset node
  1. On the Management console, select the
    Modeling
    tab.
    The Model Listing page displays the available assets.
    Select Asset for Deletion
  2. Select an asset node.
  3. Click the Delete icon.
    NOTE:
    Deletion is permanent. Once you confirm deletion, the delete action cannot be undone.
    The Confirm Deletion dialog box is displayed.
    Confirm Asset Deletion
  4. Click
    Yes, Delete
    to delete the selected asset.
    The asset and its child asset nodes are deleted upon confirmation.
    NOTE:
    If the selected asset has child asset nodes under it, upon your confirmation, all the child asset nodes including the selected asset note are deleted.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal