Delete Application

  1. On the Management Console, select the
    Applications
    tab.
    The applications list is displayed.
  2. In the
    Actions
    column, click the Delete icon next to the application that you want to delete.
    The selected application's detail page is displayed.
  3. Click
    Delete Application
    to proceed deleting the application.
    NOTE:
    Deleting an application removes all the information including the client secret. The application can no longer be used for viewing data from FactoryTalk DataMosaix. Before deleting an application, verify the information so that you delete the correct application.
    The
    Confirm Deletion
    dialog box is displayed.
  4. Click
    Delete
    .
    The application is removed from the applications list.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal