Setting up Power BI Service using the Power BI Gateway

The steps for setting up Power BI Desktop are a pre-requisite for setting up a gateway connection.
Perform the following steps for setting up Power BI service using the Power BI gateway:
  1. Install the Power BI data gateway (standard mode or personal mode) application in your system.
    Tip: Click here to download the Power BI on-premises data gateway.
  2. Open the Power BI data gateway (standard mode or personal mode) application.
    PowerBI Gateway
  3. In the left menu, click the
    Connectors
    tab.
  4. In the
    Load custom data connectors from the folder
    field, provide the exact location of the downloaded connector file (DataMosaix.mez).
  5. Click
    Apply
    .
  6. In the dialog box, click
    Apply & Restart
    to apply the changes.
    After the restart, you will be able to see the updated connector file in the Connectors tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal