Configuring Tableau to connect to a DataMosaix project

DataMosaix has an egress data interface that makes it easier for select Business Intelligence (BI) tools to build reports and dashboards based on contextualized data.
This egress data interface is exposed as a virtual PostgreSQL server that emulates a real Postgres server, and it currently supports Tableau Desktop and Tableau Server (refer to the following details). This section explains how to connect these tools to a FactoryTalk DataMosaix project. After the configuration is performed and the connection is established, users can run SQL queries directly from supported tools.
NOTE:
For more information on Cognite-related documentation, see Assets tag and Timeseries tag.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal