Delete Role 
    Perform the following steps to delete a role:
- Navigate to theRoles Listingpage and click the role you want to delete.TheRole Detailpage of the selected role is displayed.
- ClickDelete Role.TheConfirm Role Deletion?dialog box is displayed. If there are any associated apps or users with the selected role for deletion, you will be able to view a checkbox to acknowledge the removal impact.
- Select theI acknowledge deletion impactcheckbox.NOTE:When you delete a role, it will be removed from the associated apps and users. Before deleting a role, verify the details so that you delete the correct role.
- To verify the role deletion, provide the role name in theRole Namefield.
- ClickDelete Role.To make sure your changes to Roles take effect immediately, log out and log back in.
Provide Feedback