Default Roles 
    There are seven predefined roles. These are designed to give a starting point for an implementation. The following table displays the list of default Roles and the associated capability groups.
| Default Role name  | Default Capability Groups  | 
|---|---|
| Application Developer | FTDM-Grp-Applications | 
| Applications  | FTDM-Grp-GenApplications, FTDM-Grp-Experimental-Machine | 
| Application User | FTDM-Grp-ViewApp | 
| Data Configurator | FTDM-Grp-DataSetsManagement, FTDM-Grp-Function, FTDM-Grp- Pipeline, FTDM-Grp-DataModel | 
| Data Scientist | FTDM-Grp-ContextDiag, FTDM-Grp-3D, FTDM-Grp-Data, FTDM-Grp-Raw, FTDM-Grp-Chart, FTDM-Grp-Media, FTDM-Grp-Experimental-Human, FTDM-Grp-ContextEntity | 
| Extractors | FTDM-Grp- Extractor | 
| Project Admin | FTDM-Grp-Project FTDM-Grp-CognlteApllnputValidations, FTDM- Grp-AccessManagement | 
Provide Feedback