Create a Custom Role 
    Perform the following steps to create custom roles in 
FactoryTalk DataMosaix SaaS
: - On the Management console, select theManage Accesstab.
- ClickRoles. TheRoles Listingpage displays the roles associated with the selected organization.
- Click the [ ] icon.TheRole Detailpage is displayed.Role Detail Page ] icon.TheRole Detailpage is displayed.Role Detail Page 
- In theInfopane, provide the following information in the relevant fields.- Role Name
- Description(Optional field)
 
- ClickAdd Capability Group.NOTE:When you create a new custom role, it will not have any capability groups associated with it and "No Capability Group applied. Please add a Capability Group" message is displayed.TheAdd Capability Groupdialog box is displayed.
- From theBrowse Capability Groupdrop-down list, select the required group. You can also search for capability groups in the search field by typing the first characters of the capability group name. You need to select at least one capability group.TheAdd Capability Groupdialog box displays the capabilities and applied actions associated with the selected capability group.
- ClickApplyor clickApply and Add Anotherto apply the changes to the role and to add another capability group.After applying the changes, theRole Detailpage displays the added capability group(s) as a tile with the capability group name, short description, capabilities associated with the group, and the applied actions (on the right pane).
- NOTE:You need to save the changes on theRole Detailpage in order to add the capability group successfully to the selected role.
- ClickSave.
- Or,ClickSave and Add Anotherto save the changes to the selected role and start creating another role.NOTE:To make sure your changes to Roles take effect immediately, log out and log back in.
Provide Feedback