Remove Roles from Multiple Members
If you are a project administrator, you can remove assigned roles from multiple members using this feature.
Perform the following steps to remove roles from multiple members:
- On the Management Console, select theManage Accesstab.
- To remove roles from multiple members, select the checkboxes adjacent to the members' names.The [+] and [
] icons above the member grid are enabled or disabled based on the roles assigned to the selected members.- If no roles are assigned to any of the selected members, the [+] icon is enabled and [
] icon is disabled. - If all the roles are assigned to all the selected members, the [+] icon is disabled and [
] icon is enabled. - If some roles are assigned to any of the selected members, then both, the [+] and [
] icons are enabled.
- Click the [
] icon above the Member Namecolumn.Bulk Remove Roles from Members
TheRemove Rolespage displays the list of available roles with a number next to each role name. The number in the parentheses denotes how many members out of the selected members are currently assigned to a role. The user can click the number in the parenthesis to view the assigned member details.Members Assigned to a Role
- Select the checkboxes adjacent to the roles you want to remove. Selecting the checkboxes will remove those roles from the members that are currently assigned the roleNOTE: The user can use the search bar to find a specific role.You can remove all the assigned roles, by selecting theRolesheader checkbox.
- ClickRemove.The "Roles updated" message is displayed.Bulk Remove Roles
NOTE:- Click the [
] icon to expand the role and view its capabilities. Click the icon again to collapse it.Role Capabilities
- If the Project Admin role is selected, then theConfirm Role Removal?dialog box is displayed.
- The Project Admin role cannot be removed from a member who is either an owner/ Project Admin inFactoryTalk Hubor is the only member in the organization with the Project Admin role.
NOTE:
For more information on CDF Access Management, refer to this link.
Provide Feedback