Set Client Credentials for Transformation
Perform the following steps to set client credentials for transformation:
- In the Mapping editor, clickRunand selectRun with client credentials.If the client credentials are not set, you can view the missing credentials dialog box. You need to set your client credentials before you can run a transformation.Mapping Editor

- ClickSet client credentials.Missing Credentials Dialog

- On theClient Credentialsdialog box, provide the client credentials that you saved when you registered an extractor earlier.Set Client Credentials
Then, you are ready to run the transformation.
Provide Feedback