View Newly Create Assets

Perform the following steps to view the newly created asset:
  • FactoryTalk DataMosaix SaaS
    : On the Management Console, click the
    Modeling
    tab to view the newly created assets.
    Model Listing
    TIP:
    If you can view the newly created assets on the Model Listing page, click the Refresh [ ] icon to update the page.
  • Cognite Data Fusion: Navigate to
    Data Explorer
    >
    Assets
    .
    Assets
  • When you run the connector, you will view the Flexible Data Models
NOTE:
When the user runs the connector using the extractor config file, the extraction pipeline is updated with the associated dataset to track the extractor's run history and the current status of the pipeline.
Extractor Run History
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal