Store and Forward Data
The Store and Forward in
FactoryTalk Optix
stores data in a S&F queue to store data locally when the FactoryTalk Optix
project encounters an issue or stops functioning. When this queue reaches its configured limit, the queue is pushed to a disk file. Therefore, the Store and Forward data is retained in both a memory-based queue and on a disk file. Once the connection is restored, the stored data is retrieved and pushed into the CDF, ensuring that no data is lost.In the Store and Forward Data, the MaximumQueueLength property defines the maximum number of batched datapoints that can be pushed to the StoreAndForward queue. When the number of items (batches of datapoints) exceeds this limit, the items will be stored to the disk file. Additionally, the MaximumFileSize(KB) property defines the maximum size of the file used to store data. When this limit is reached, store and forward will stop storing data.
NOTE:
An error message is displayed if the actual file size exceeds the available free space on the disk.
Data cannot be stored directly in S&F. A successful connection must be established first in order to store data in Offline mode.
Perform the following steps to configure the maximum limit of a memory-based queue:
- Open theFactoryTalk Optix Studio.
- Navigate toDataStores>FTDataMosaixDataStorefrom the left pane.Select FTDataMosaixStore

- In thePropertieswindow, perform the following actions:
- Provide a value greater than or equal to 1 for theMaximumQueueLength.
- Provide theMaximumFileSize(KB). This should be set to a value based on available disk space on the machine where theFactoryTalk Optixproject will be deployed.Store and Forward

When the connection is interrupted, the data will start storing in the text file.
Storage Location

NOTE:
The text file will be stored in the project application directory.
The following image displays that no data is pushed into the CDF:
No Data in CDF

When the connection is restored, all data from the text file will be pushed to the CDF. The following image displays that all the data is pushed into the CDF:
Data in CDF

NOTE:
The text file stored locally will be deleted automatically.
Provide Feedback