Run the FactoryTalk Optix Project in Optix Panel Runtime

To run the
FactoryTalk Optix
project in the Optix Panel runtime, the user needs to configure the Optix Panel in
FactoryTalk Optix
.
Perform the following steps to configure the
Optix Panel
in
FactoryTalk Optix
:
  1. Click the
    Emulator
    drop-down list and click
    Local
    .
    Drop-down Selection
  2. Click the [+] icon to add new target device.
    Add New Target Device
  3. Provide the following details:
    • Name: Provide name of the target device.
    • IP Address: Provide the IP Address of
      FactoryTalk Optix
      Panel.
    • Username: Provide the username of
      FactoryTalk Optix
      Panel.
    • (Optional) Destination Path: Provide the target device deploying destination path.
  4. Select the
    Encrypt project
    ,
    Transfer source project
    ,
    Transfer application files
    , and
    Transfer optimized project
    checkboxes.
  5. Click
    Select
    .
    FTOptixStudio Window
  6. Place the
    config.yml
    file in the
    project directory > ProjectFiles
    path. Default path is
    C:\Users\<Username>\AppData\Local\Rockwell Automation\FactoryTalk Optix\Emulator\Projects\AlramSnF\ProjectFiles
    Copy Config File
  7. Provide the config file path as
    %PROJECTDIR%
    .
    ConfigFolderPath
  8. Follow the steps from the above section (
    Configuring FactoryTalk Optix to Connect to FactoryTalk DataMosaix SaaS – Continuation
    ).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal