Edit Extractor
Perform the following steps to edit extractor:
- On the Management Console, select theExtractor Infotab.The Extractors list is displayed.Extractor Listing

- In theActionscolumn, click the Edit icon next to the extractor that you want to edit.TheExtractor Detailpage is displayed.Extractor Detail screen
You can edit the extractor information such as Source Name, Location, Associated Roles (Only for Project Admin users can view and edit), Pipeline, and Source Type. - Edit the information in the required fields.
- ClickDownload Configurationto download the configuration file in .yml format.
- ClickSave and Apply.
Provide Feedback