Regenerate Secret for Application
    
     NOTE: 
    
The following instructions apply only to Machine to Machine applications.
- On the Management Console, select theApplicationstab.TheApplications Listingpage is displayed.Application List 
- In theActionscolumn, click the Edit icon next to the application for which you want to regenerate the client secret.Edit icon The Application detail screen displays with the existing client secret and theRegenerate Secretlink.Regenerate Secret Link The Application detail screen displays with the existing client secret and theRegenerate Secretlink.Regenerate Secret Link 
- Click theRegenerate Secretlink.A message displays waiting for confirmation to regenerate secret.Regenerate Client Secret Confirmation Box NOTE:Generating a new client secret makes the existing client secret invalid. After generating the new secret, you must update the client secret information in the required files. NOTE:Generating a new client secret makes the existing client secret invalid. After generating the new secret, you must update the client secret information in the required files.
- ClickYes, Regenerate.TheApplications Detailpage displays the new client secret.New Client Secret 
- ClickCopy Secretto copy and save the new client secret.- Open a text file, paste the new client secret, and save the file.
 NOTE:It is important to copy the client secret and update it in the related files. Once you close this screen, this information cannot be viewed later. If you fail to save the client secret information, you will have to regenerate the secret.
- ClickDone.
Provide Feedback