Edit Application
- On the Management Console, select theApplicationstab.TheApplications Listingpage is displayed.Applications Listing

- In theActionscolumn, click the Edit icon next to the application that you want to edit.The selected application's detail page is displayed.Edit Application screen
You can edit the application information such as Application Name, Application URL, and Description. In case of Machine to Machine application, you can also edit Associated Roles. - Edit the information in the required fields.
- ClickSave Changes.TheApplicationstab displays the updated information for the edited application.
Provide Feedback