Delete Application
- On the Management Console, select theApplicationstab.The applications list is displayed.
- In theActionscolumn, click the [
] icon next to the application that you want to delete. - TheConfirm Deletiondialog box is displayed.NOTE:Deleting an application removes all the information including the client secret. The application can no longer be used for viewing data fromFactoryTalk DataMosaix SaaS. Before deleting an application, verify the information so that you delete the correct application.
- ClickDelete.The application is removed from the applications list.
Provide Feedback