How to access FactoryTalk DataMosaix SaaS APIs via Swagger UI
- Navigate to the Swagger UI page. You can navigate to any of the following Swagger UI pages.ModuleSwagger URL
- ClickAuthorize.Authorize

- Provide a valid token.
- ClickAuthorize.Available authorizations

- Select the variables as shown in the following figure. The computed URL should be as follows.Set Variables
NOTE:The above URL is for Access management service, for other services, theHostname will be different. - Select the API that you want to test and clickTry it out. Here is an example for the Get request.Sample Get request

- Set the required parameters and clickExecute. Upon successful API call, you should get a 200 OK response.Execute API
Successful API response
Provide Feedback