Configuring the Settings
- HTTP
- Name: Update the name from the default name.
- Project: The name of the project inFactoryTalk DataMosaix SaaS.
- API Host: <ClusterName>.cognitedata.com (Host URL).The API host will dynamically change according to the cluster selected while creation of the project.NOTE:By default, the cluster selection feature flag is turned off, allowing the user to view only the default cluster (West Europe-1). To view all the supported cluster details, the cluster selection feature flag must be turned on. For more information on the supported cluster details with API URL, refer to Create Project.NOTE:The cluster list is subject to change.
- Auth: We are using OAuth2, so, enableOAuth2 client credentialsoption.
- Token URL:https://datamosaix-prod.us.auth0.com/oauth/token
- Client ID: Refer to the Client ID generated while registering the application.
- Client Secret: Refer to the Client Secret generated while registering the application.
- Scope: user_impersonation
- ClickSave & test.
- Refer to the following image for a valid configuration.Grafana Valid Configuration
NOTE:For the Bad Gateway error, check API Host written as <ClusterName>.cognitedata.com not the https://<ClusterName>.cognitedata.com. - ClickExploreto get access to the project data, you can analyze and visualize data and create the dashboard.
- For more information on Cognite Data Source for Grafana, you can refer to the documentation.
Provide Feedback