View the signature list

The
e
Procedure
Signatures List displays a list of pending signatures and their related commands, report parameters, and other data. The list of pending signatures is maintained on the
FactoryTalk Batch
Server.
TIP: Step Verification signature requests and Reactivate Step signature requests only display in the Instructions view; batch and phase command verification signature requests display in the Signature List and the appropriate
Signature
dialog box opens in the Instructions view.
Click the
Signatures
button to display the Signatures List page, shown below. Each row in the list represents one signature. The Signature List automatically updates as new signatures are generated and the states of existing signatures change.
ePro_Signature_List_view
TIP: Signatures are not filtered; therefore the Filter area and the
Select Filter
button are not available on the Signature List page.
TIP: If you do not have sufficient rights to view the Signature List, you are prompted "The current user does not have permission to view the Signature List." See the for information on configuring signature and signoff security.
The following columns display on the Signatures List view:
Column Name
Default Header
Default Width
Time
Time
120
Batch ID
Batch ID
100
Signoff Meaning
Signoff Meaning
230
Signoff Security
Signoff Security
120
Signature Context
Signature Context
250
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal