Acknowledging a signature request

Double-clicking a signature on the Signature List opens the appropriate
Signature
dialog box, from which the required signoff(s) are made or canceled. From this dialog box you can view the time and date the signature was generated, the ID of the batch, and the procedure ID and specific command that caused the signature to be generated. The dialog box shown here is a
Command Signature
dialog box generated by a HOLD command.
FTB_admin_commandsignatureHOLD
You have the option of enabling (in the
FactoryTalk Batch
Equipment Editor) a signature request on up to eleven general commands and one
e
Procedure
-specific command.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal