Prompted binding
Prompted binding is the process of binding a unit to a step after a bind prompt is generated. Only unit class aliases that are defined as having the Prompt binding method generate a prompt. This includes those that are defined with Prompt binding during batch creation. The execution of the batch pauses when the transition above the unbound step becomes True. The "Bind to Alias" prompt displays in the Instructions view.
TIP:
All other steps within the procedure that are associated with the same alias are bound to
the same unit.
- In the Batch List window, start the batch that contains the bound unit (if it is not already running).
- Select the Instructions view.
- ThePrompt to Bind Unit Aliasinstruction form opens.

- Select the unit to which the step is to be bound, and then clickOK. The prompt is removed from the Instructions view when the acknowledgment successfully completes.
Provide Feedback