Run material-based recipes without the Material Server
If communication is lost with the Material Server, material-based control recipes can continue to process. A highly visible warning message displays when communication is lost with the Material Server. When adding a material-based control recipe to the batch list without access to the Material Server, you must select the materials and containers for binding. For control recipes run without the Material Server, you must update the inventory manually in the Material Editor using the addition and distribution information presented in the Event Journal.
WARNING:
Loss of the Material Server causes the
FactoryTalk Batch
Server to switch to prompt binding and presents an unfiltered list of container/equipment module pairs from which to select binding candidates. The operator must select the container/equipment module pair to supply the correct material to continue processing the batch. Failure to select the correct container/equipment module pair could result in a hazardous situation depending on the material. Exercise extreme caution when operating without the Material Server.(See the for more information about running
recipes without the Material Server. See the for more information about updating
inventory.)
FactoryTalk Batch
Material Editor User
Manual, publication BWMTR-UM001Provide Feedback