Confirm report values
Report parameters can be defined to include range checking. The report parameter can require confirmation for values outside a specified range. Report parameters can also be defined to require the report value to be within a specified range, forcing the operator to correct an entry that is outside the range. The
Confirm Value
dialog box is generated from the HTML code.
- If the report value is valid, you can enter an optional comment and then clickOK.
- If the report value is incorrect, click theCancelbutton to cancel the submit process and return to the current control step where the value is selected. You can then enter the correct report value and re-submit the report data.
(See the for information on including
Confirm and Comment instructions in control steps.)
Provide Feedback