Information in the Equipment view
The Equipment view presents a set of data based on the selected level. Additional Phase Logic Interface (PLI) information is displayed as a tool tip when your cursor passes over an equipment module. The following is an overview of the data displayed within each level:
Information | Description | Area | Process Cell | Unit | Phase |
|---|---|---|---|---|---|
Batch ID | The Batch ID of the selected batch. In the Area display mode, there is a
drop-down list containing the Batch IDs of all the batches on the Batch List in
order by Create ID. | X | X | X | X |
State-SI | The state of the phase along with the step index; only included in the Unit
display mode. | X | |||
State | The state of the selected batch. For example, RUNNING, HELD, etc. | X | X | X | X |
Mode | For the Area and Process Cell displays, this is the mode of the selected batch.
For example, O_AUTO, MANUAL, or S_AUTO. In the Unit display mode, this indicates
ownership of the phase. For example, PROGRAM if the phase is under a batch's
control, OPERATOR if the phase has been acquired by the operator and EXTERNAL if
the external bit has been set. | X | X | X | X |
Instructions | A link to the Instructions view. The instructions for the current batches within
the area or process cell are included in the Instructions view. | X | X | ||
Link1 - Link5 | These customizable hyperlinks can be defined for each equipment resource in the
equipment database. The labels (Link 1, Link 2, etc.) are also customizable for
each specific equipment resource type. | X | X | X | |
Request | A description of the unresolved request on the phase, if any. | X | X | ||
Phase | The name of the phase. | X | |||
Step Index | The step index of the phase. | X | |||
Failure | Failure message, when appropriate. | X | |||
Unit | Name of the unit in which the phase resides. | X |
Provide Feedback