Start a material-based phase

  1. Acquire the appropriate phase.
  2. Click the
    Start
    button to initiate the phase. The
    Phase Control Feed Type and Material Selection
    dialog box opens.
    ePro_mbr_mpc_feed_type
  3. Select the
    Feed Type
    (if available), and
    Material
    , and then click
    OK
    . The
    Phase Control
    dialog box opens.
    ePro_mbr_mpc_container_type
  4. Type a unique
    Batch ID
    for the manual phase control batch in the
    Enter Batch ID
    box, unless you are generating Batch IDs automatically.
    (See
    Batch identification
    in the for more information.)
  5. Select the appropriate container from the
    Make a selection to bind equipment module
    box and click
    OK
    . The State changes to RUNNING.
    TIP: The first container on the list is the default container.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal