Hyperlinks
Equipment
includes up to five hyperlinks for each process cell,
unit, and phase shown. In the diagram view, find the hyperlinks near the equipment icon.Using the Equipment View Hyperlink feature with
FactoryTalk Batch View
requires changing the location of the files to link to the
appropriate FactoryTalk Batch View
directory.
TIP:
Define the hyperlink descriptors and defaults in the for more information.
FactoryTalk
Administration Console Explorer
. Right-click an application or area name to
either add a server or edit an existing one. To add a server, select . Configure the hyperlinks in the FactoryTalk Batch Services
Properties
dialog > Descriptors and Defaults
tab
> Hyperlink descriptors and defaults
area. See the FactoryTalk Batch
Administrator's User Manual
, publication BATCH-UM003
To create a hyperlink folder in the
FactoryTalk Batch View
directory- In File Explorer, navigate to theFactoryTalk Batch Viewweb root directory. IfFactoryTalk Batch Viewis installed in the default location, the directory is:C:\Program Files (x86)\Rockwell Software\Batch View Server\customercontent.
- Create a new folder and enter a name for the folder (such asProject_Files).
- Put the files to link in this folder.
- InFactoryTalk Batch Equipment Editor, make sure that the path configured for the hyperlink matches the directory path created in step 2 (such ascustomercontent/Project_Files/<file name>).
Provide Feedback