Stop a batch

The STOP command is used to permanently stop the execution of a batch at the current step in a non-emergency situation. A batch can be stopped from the following
FactoryTalk Batch View
windows:
  • Batch List view
  • Procedure as SFC view
  • Procedure as Table view
    IMPORTANT:
    You
    cannot
    restart a STOPPED batch.
To stop a batch:
  1. In the
    Batch List
    view, select the batch.
  2. (optional) In the toolbar, click
    Procedure as SFC
    or
    Procedure as Table
    to select the view you want.
    1. Select the step you want to stop.
    2. The mode must be O-AUTO.
  3. Click
    Stop Batch
    or
    Stop Step
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal