Place a batch in automatic mode
A batch or step that is in MANUAL mode must be placed in AUTOMATIC mode to continue normal execution. A batch or step may be placed in AUTOMATIC mode from the following Client views: Batch List, Equipment and Procedure.
e
Procedure- Open the appropriateClient view.eProcedure
- Use the Filter view to select the batch that is to be placed in AUTOMATIC mode. To place the entire batch in AUTO mode, you should select the highest recipe level and place it in AUTOMATIC mode (i.e., unit procedure or procedure).
- Click theAutocommand button. The batch will continue to sequence automatically.
- All higher level steps are left in MANUAL mode and all lower level steps are placed in AUTO mode.
Provide Feedback