Hold a batch

This command temporarily stops execution of the batch at a step. A HELD batch can be RESTARTED, STOPPED, or ABORTED. A batch can be held from the following
FactoryTalk Batch View
windows:
  • Batch List view
  • Procedure as SFC view
  • Procedure as Table view
To hold a batch:
  1. In the
    Batch List
    view, select the batch.
  2. (optional) Click
    Procedure as SFC
    or
    Procedure as Table
    to select the view you want.
    1. Select the step you want to hold.
    2. The mode must be O-AUTO.
  3. Click
    Hold Batch
    or
    Hold Step
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal