Use the Batch List view
The Batch List view provides an overview of the batches that are running, ready to run, or complete. The Batch List view is used to create and command batches. A batch remains on the Batch List until you remove it or until the
FactoryTalk
Batch Server is restarted with a cold boot.
Batches are specific instances of the master recipes developed for your facility. When you create a batch you may be prompted to select or input parameter values, and/or to select specific units in which the batch will run.
TIP:
If you are running Internet Explorer version 7.0 or
higher, it is possible to have multiple instances of the Client
running in the same browser window. The current user will be logged on to all instances.
(See
e
ProcedureRunning on Internet Explorer version 7.x
for more information.)Provide Feedback