OPC group support

Within the OPC protocol, data is accessed through collections of data items referred to as groups. Different data servers have varying levels of OPC support, including maximum numbers of groups, maximum numbers of items per group and performance issues, and so on. Because of this,
FactoryTalk Batch
support of OPC is flexible in order to achieve successful communication with as many different data servers as possible. To achieve this, the
FactoryTalk Batch
Server is flexible in its definition of Groups, and allows for different OPC grouping configurations to communicate with the data server(s).
The manner in which the
FactoryTalk Batch
Server organizes the area model tags into groups is defined by data server definition files (DSDF). These files are located in the Batch\Dataservers directory.
FactoryTalk Batch
comes with a predefined set of DSDF files. If you need to communicate with a data server for which there is no predefined DSDF file, contact
Rockwell Automation®
Application Support.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal