Performance chart

The performance chart included with
FactoryTalk Batch
is a pre-defined set of charts for use with the Windows System Monitor.
TIP:
The predefined performance monitor charts are in English only. Non-English customers must configure the charts manually. (Refer to your Windows documentation for more information on performance charts.)
The System Monitor can examine the use of computer resources by
FactoryTalk Batch
components, as well as other processes and applications, and it can help determine if a process or application is using too much CPU time or memory. The pre-defined Performance Chart, supplied with
FactoryTalk Batch
, charts specific processes that can affect the performance of
FactoryTalk Batch
, and can be an important tool in identifying and troubleshooting system problems.
TIP:
The performance chart is intended to be used primarily as a debugging and diagnostic tool by
FactoryTalk Batch
product support personnel.
The Windows System Monitor is used to view chart data, alerts, logs and reports. Additionally, charts can be saved for future review. To view the
FactoryTalk Batch
performance chart, make sure that the System Monitor is set to chart view mode
.
(Refer to your Windows documentation for more information on using the System Monitor.)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal