Objects embedded in HTML code do not display

By design, the eProcedure service does not look for embedded objects in the manual instruction files (HTML template). The service simply passes that HTML code through to the Client and allows the browser to interpret it. All embedded objects must be available from a secure (HTTPS) web server. The
FactoryTalk Batch View
Server can host the content in Batch View Server\customercontent folder. By default the location of this folder is:
C:\Program Files (x86)\Rockwell Software\Batch View Server\customercontent
TIP:
Make sure the object’s HTML code occurs within the <form> tags in the instruction file.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal