FactoryTalk Batch Phase Simulator interface

Upon startup, the
FactoryTalk® Batch
Phase Simulator reads the area model that is specified in the
Area Model
path that is defined in
FactoryTalk Administration Console
FactoryTalk Batch Services Properties
Project Settings
Server directories
. The area model file name is displayed on the title bar. By default, when you first install the software it is set up to read
ice_cream1.cfg
, one of the sample area models shipped with
FactoryTalk Batch
. This file contains the equipment required to run the Sampledemo1 recipe. The Simulator simulates the RUNNING, STOPPING, HOLDING, ABORTING, and RESTARTING states for all phases configured in the recipe.
FTB_Admin_Simulator
TIP:
The Simulator simulates only phase states for area models that have no more than 50 parameters and 50 report parameters.
The Simulator menu bar consists of these options:
Options on the Simulator menu bar
Option
Definition
File
Open a simulator (.sim) file, save a file, or exit the Simulator.
Edit
Edit phase configuration, phase status, or unit tag status.
Protocols
Enable or disable the Watchdog and Command Handshake functions.
Help
Open the Simulator
About
box.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal