Restore and clear requests

Requests generated by a phase can be stored in the request buffer registers should the phase receive a Hold command. The requests can then be copied back to the request registers when the phase receives a Restart command. The
Restore Req
and
Clear Req
registers must both contain a
1
(one) to allow for the saving and restoring of requests for a HELD/RESTARTED phase.
To restore and clear requests:
  1. Start the
    FactoryTalk Batch Phase Simulator
    .
  2. Select
    Edit > Phase Status
    .
  3. In the
    Select Phase
    list, select the phase to command.
  4. In the
    Restore Req
    register, type a
    1
    .
  5. In the
    Clear Req
    register, type a
    1
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal