Change ownership of a phase

The
Owner
button acts as a toggle, switching the value in the
Owner
register between zero and one. A zero represents Batch as the owner and a one represents an external owner.
To change ownership of a phase:
  1. Start the
    FactoryTalk Batch Phase Simulator
    .
  2. Select
    Edit > Phase Status
    .
  3. From the
    Select Phase
    list, select the appropriate phase.
  4. To set ownership to
    External
    , select
    Owner
    when the value in the
    Owner
    register is
    0
    .
    To set ownership to
    Batch
    , select
    Owner
    when the value in the
    Owner
    register is
    1
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal