Acknowledge and clear a request
Requests must be acknowledged and then cleared to allow a phase to continue processing when running under External control. The
Ack/Clear Request
button must be clicked twice, first to acknowledge the request, then to clear the request.To acknowledge and clear a request:
- Start theFactoryTalk Batch Phase Simulator.
- SelectEdit > Phase Status.
- In theSelect Phaselist, select the phase to command.
- If theRequestregister contains a request, selectAck/Clear Requestto acknowledge the request. The value in theRequestregister changes to10, indicating that the request confirmation was received from the Batch Server.
- SelectAck/Clear Requestto clear the request. Upon clearing the request, the value in theRequestregister changes to0, indicating that the request was cleared. The phase continues to process.
Provide Feedback