Indicate a continuous phase
Simulate continuous phase logic by selecting
Continuous Phase
.To indicate a continuous phase:
- Start theFactoryTalk Batch Phase Simulator.
- SelectEdit > Phase Configuration. ThePhase Configurationdialog box opens.
- From theSelect Phaselist, select the appropriate phase.
- If this is a continuous phase, selectContinuous Phase.
- SelectUpdate Phase.
- SelectClose.
Provide Feedback