Change the sequence of requests
Change the time, type, and parameters of the request in a phase.
To change the sequence of requests:
- Start theFactoryTalk Batch Phase Simulator.
- SelectEdit > Phase Configuration.
- In thePhase Configurationdialog box, from theSelect Phaselist, select the appropriate phase.
- Type an appropriate value in@Time(time is in seconds). This value determines when the request is processed. This value must not be greater than theDwell Time.For example, if theDwell Timeis 30 seconds, and the@Timevalue is 20 seconds, then this request will be processed after the selected state has been active for 20 seconds.
- Type an appropriate request number in_RQ. (Refer to the for information on request numbers.)
- Type any required request parameter data inQ01,Q02, andQ03. These parameters are used to further define the request.
- Select theUpdate Phasebutton.
- SelectClose.
Provide Feedback