Change the dwell time

Change the length of time that a specific state is active for the selected phase.
To change the dwell time:
  1. Start the
    FactoryTalk Batch Phase Simulator
    .
  2. Select
    Edit > Phase Configuration
    . The
    Phase Configuration
    dialog box opens.
  3. From the
    Select Phase
    list, select the appropriate phase.
  4. From the
    Select State
    list, select the state to change the dwell time.
  5. In
    Dwell Time
    , type the desired dwell time for the selected state.
  6. Select
    Update Phase
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal