Open the
e
Procedure
Client

The
e
Procedure
Client runs in Internet Explorer. The
FactoryTalk Batch
Server and
e
Procedure
services should be running prior to opening the Client. If configured properly, Internet Explorer can use the
e
Procedure
Client as the home page so that when you open Internet Explorer the
e
Procedure
Client opens.
(See the for more information.)
TIP: By default, the
FactoryTalk Batch
Server starts automatically when the computer is started. The
FactoryTalk Batch
Server and
e
Procedure
Server must be running before opening the
e
Procedure
Client.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal