e
Procedure
Client views

The
e
Procedure
Client provides information regarding current batches and the facility’s equipment in five unique views. Each view displays different information. The information displayed is based on the current filter, except for the Batch List and Signature List views, which present information unfiltered. Each view also allows for the issuing of commands to the batch.
  • Batch List view
    Enables the operator to create and command a batch. A batch remains on the Batch List until the operator removes it, or the
    FactoryTalk Batch
    Server is restarted with a cold boot. See
    Using the Batch List view
    for more information.
  • Equipment view
    Provides a graphical view of your facility’s equipment. The Equipment view displays run-time information that is relevant to the type of equipment displayed. You can use the predefined hyperlinks to access custom Web pages, documents, or applications. See
    Using the Equipment view
    for more information.
  • Procedure view
    Provides an SFC view and a Table view of the selected batch, unit procedure or operation. The Procedure view allows you to command any portion of the batch, from the procedure level down to the phase level. See
    Using the Procedure view
    for more information.
  • Instructions view
    Provides the ordered list of control steps for the selected filter. You can view Current, Past and Future control steps. See
    Using the Instruction view
    for more information.
  • Signature List view
    Displays a list of pending signatures and their related commands, report parameters, etc., which are maintained on the
    FactoryTalk Batch
    Server. See
    Using the Signature List view
    for more information.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal